This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sirs,
Would you pls advise if the noise floor measurement in line with the PCM2912A's specification? I added AES127 software filter and 10kOhm load impedance
Played 0dB FS, 1kHz sinewave with maximum volume, Got 685.8mV rms (-3.275dBV) as full scale output voltage.
Play silence file, Got 42.76uV (-87.867dBV) as PCM2912AEVM's noise floor. The noise level is audible -> Was it in line with PCM2912A's specification?
Stop playing media file, Got 24.07uV (-93.836dBV) as PCM2912A EVM's shutdown mode.
Hi, Wayne,
The value obtained is close to the expected performance of the device, there are a couple points to consider with this measurement:
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Wayne,
I think that whenever Windows stops playing audio, the USB bus becomes idle, so the PCM2912A shuts-down the output stage.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer