This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM2707C
Hello.
Our customer have a project like Amazon Echo applitacion. I need to check the voice control function BD on below with yours.
We have 8-ch MIC input to two PCM1864. Our question is PCM2707C can support I2S input to USB output or not?
And Below BD is ok or something need to modify. Thanks for help~
HI, AJ,
The PCM2707C USB audio DAC is capable of operating in I²S mode, but the output of the I²S interface is sent to the DAC input of the device, there is no USB output from this device. Also, the USB interface if this part doesn't support TDM, so only two channels are supported.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer