This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM2707C
Dear Expert,
We design PCM2707C as audio DAC. But now we face an issue, usb host cannot found PCM2707C device.
All the power rail and x'tal are working fine. Schematic as below.
Is there any risk in my schematic? Please give me your feedback about this issue.
Thanks!
Hi, Ben,
If the device is properly powered it should be detected by the host as this part uses the native USB Audio driver of the OS. The schematic seems overall ok, however, it seems some resistors in D+ and D- are missing, are they in a different section of the schematic?.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Ben,
Thanks for the feedback. This is not normal, the part should be automatically detected by the host device. Have you tried to bypass the hub to see if the PCM2707C is identified properly by the host system?.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Ben,
As you mention, Vbus should be connected to VDD when the device is set in self-powered mode. You need to make sure PSEL pin is configured to put the part in self-powered mode (PSEL=0) before connecting Vbus to VDD. On the schematic, PSEL = 1, which means the device is set to work in Bus-powered mode.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer