hello
I Have used the PCM5242RHBEVM + TPA3244EVM, and when input with Coaxial SPDIF or Optical, there is no output.
I have followed the jumper setting as configulation tab, but it also no output. so what should I do next? thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello
I Have used the PCM5242RHBEVM + TPA3244EVM, and when input with Coaxial SPDIF or Optical, there is no output.
I have followed the jumper setting as configulation tab, but it also no output. so what should I do next? thanks~
Hi Kevin:
I have found the I2C Command to solve the problem in E2E, Thanks~
https://e2e.ti.com/support/data_converters/audio_converters/f/64/p/501935/1818532#1818532
And I have applied PP3 request for 3 time, but No reply yet. So I only can use the I2C Master to control the PCM5242EVM....