This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have enjoyed reading tidu765. I am working on a design to try to detect a 50-100 hz signal based on this design reference.
Has anyone modified tidu765 to run on a 3.3v supply? Is this a bad idea? I can always add a boost to 5v, but am looking to minimize hardware. If this isn't a terrible idea, can anyone provide some good first steps / pitfalls that I should be aware of?
Thank you!
Hello Noah,
The circuit shown in TIDU765 can be modified to work at +3.3V. However, the OPA172 that was used in the design requires a minimum power-supply voltage of +4.5V, so you'll need to select a different op amp to work at +3.3V.
Consider the TLV9062, TLV6741, or OPA377 products.