Other Parts Discussed in Thread: LM48100Q-Q1, TAS2505-Q1, TAS2505
Hi Team,
This question is related to my post on the audio converters forum:
I'm trying to architect a system that has two I2S inputs and a single mixed mono output. I'm looking for something that has short circuit and open load detection, like the LM48100Q-Q1. Can the TAS2553 do short circuit and open load detection with the IV sensing? I searched around the datasheet but didn't see any mention of it. My thought is it potentially use two of these tied together for a single output. If this won't work, is there another amp that's a better option? Some way of doing either two I2S inputs (with 1 or 2 chips) or a single analog input (which would take in the premixed signal) would work.
Thanks!
Nate