This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5508-5122C6EVM - Is input board included?

Other Parts Discussed in Thread: TAS5352, TAS5342, TAS5631

Hello,

 

I am hoping to track down the TAS5508-5122C6 Evaluation kit, and am wondering if the TI-input board is included with the kit.

The literature makes plenty of references to it, but doesn't explicitly say that it is included.

Do you know if it is included?

 

Thanks,

 

Matthew

  • Hi, Matthew,

    Yes, the input board and cables to connect it to the EVM itself should be included. There may or may not be a cd rom with the s/w on it, if not, the software is available in the Product Folder on the web to download.

    That is a pretty old part; I might recommend you look at some of our newer ones like TAS5342 and TAS5352 and TAS5631.

    -d2