Other Parts Discussed in Thread: TAS5414C, TAS5414CQ1PHDEVM
DigiKey delivered today my TAS5414CQ1PHDEVM evaluation kit for the TAS5414C. Thanks. Well done kit.
Quick feedback to TI: I need to rebuild the USB2IIC2 interface board that is part of this kit because TI's packing method resulted in several through-hole parts being ripped out of their landings. The kit had not been roughly shipped, but the compression-between-foam-blocks packing method apparently allows the anti-static bag to roll around in the box.
No big deal. I have the parts here to repair the USB2IIC2 board.
However, I would like to have the Altium Designer CAD files pertaining to the amplifier board itself. In the downloadable data sheet for the eval kit there are PDFs of some layers of this board, but at 1:1 scale these PDFs are useless. And the images are highly "de-res'ed" from the original drawings. I can barely read the schematics due to the Acrobat compression.
A good place for these CAD files would be in the ZIP file in which the downloadable GUI arrives, but I found none there.
BTW, I notice that the GUI code is labeled Rev. 2. Does the Rev. 2 driver run under something newer than Windows XP?
Thanks.
Jim Olson/Radian Research/ Lafayette, IN US