Other Parts Discussed in Thread: TLV320ADC3101, PCM1789
Hi Team
we are using this DAC part in our design All the digital signals are driven from the processor to the DAC and the DAC is interfaced to the PA TAS5421QPWP. Generally, we separate the And and Dgnd in DAC
if we need to do we should connect the DGND to the digital GND but in the datasheet, both are connected to a common AGND Can I connect this DGND pin to the Digital GND Since VDD is connected to the digital supply if the analog audio outputs are connected to TAS5421QPWP Which ground should this Use
This is the Current schematics that we have