This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
The location of beep generator as below, right?
we found the abnormal signal when we play 1KHz by beep(On customer unit).
However, when we play 1KHz.wav, the signal is normal.(On customer unit)
We guess that issue from the beep generator…, do you have idea about it?
Thanks, Ian.
Dear Steve,
However, I measured the signal from evaluation kit, it is smooth from below beep generator…
Any I misunderstanding?
Thanks, Ian.
Dear Steve,
Here is the setting of the codec related clock… have any comment? Thanks!!!
CLOCK |
Frequency |
|
Single tone by beep generator |
Audio playback (1KHz.wav file) |
|
MCLK |
25M Hz |
25M Hz |
WCLK |
48K Hz |
44.1K Hz |
BCLK |
1.53MHz |
1.41MHz |
Signal |
Stepping sine waveform |
Normal sine wave |
Thanks, Ian.
Dear Steve,
Got it, so, have the distortion from beep generator, for example, when playing 10KHz tone from beep generator, but we listen may not like an 10KHz tone, that’s what I want to confirm…thanks
Thanks, Ian.
Ian,
Download Purepath Studio, This will allow you to program the MiniDSP. you will need to put together some kind of process flow. I assume they will still want to mix the Audio from the ADC, the Audio from the I2S and the Tone?
once they create a process flow they can Build the project, and generate the code. the tone generator block has 3 runtime properties - status, Frequency, and Amplitude.
if frequency and Amplitude are constant, they the status register is all they will need to change.
I've taken a quick screenshot of the Tone Generator block and its properties. let me know if you need some help getting the miniDSP programmed. I assume you have used Purepath Studio before?
best regards,
-Steve Wilson