This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Guys!
I have two questions related about output of TAS5631 or TAS5630 apply at a Automotive Class D Power Audio Amplifier:
1) Since the NXP part TDF8591 works with simetrical power supply they works with the wave from -12V to +12V excursion so it’s more resistant to automotive noise. In the case of our device how we can work on that??? Needs to be grounded??
2) The second question is a little bit related with the first one: here is common works in 2 Ohms Speakers (per output) in a 4 channel output module and the final customer used to do half bridge or full bridge (PBTL). A example, a amplifier with 4 channel 100W output the customer connect (short-circuit/PTBL) 2 channels in bridge to have 200W output. Can we do the same with our device??
If the both questions are yes? Did you have a schematic of that??
Thanks in advance!!
Marcelo
Marcelo, TAS5630 and TAS5631 work from a single grounded supply (please review pages 17-21 of data sheet SLES220B). But I do not believe that the dual supply for TDF8591 (+/- 12 to 30 V) gives it high immunity to power supply noise. S/E configurations inherently have lower supply immunity than differential configurations. (See attached presentation "APA-ClassD-op-meast-100818.pdf").
TDF8591 requires higher supply voltages than +/-12V to produce 100W, even S/E with 2ohm load. (Page 13 of TDF8591 data sheet.) TDF8591 requires both positive and negative switching supplies for reasonably high power. In contrast, TAS5630 and TAS5631 work from a single grounded supply, so their power supply is simpler than TDF8591's. The voltage still must be higher than 12V, but only one switching supply is required.
I am not sure I understand your second question. Please review pages 4, 9 and 10 of data sheet SLES220B regarding load impedances and output power in S/E, BTL and PBTL configurations. I hope this will answer your question.
Regards,
Steve.
Marcelo, I intended to attach a PDF above, and I have done this now. If you downloaded it, please delete the PPT and do not distribute it to anyone.
Best regards,
Steve.