This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5634: Need Power Stages to Support 400W at 2ohm PBTL / 200W at 4ohm BTL

Part Number: TAS5634

Hi Sirs,

Do we have a power stage to support load conditions of 400W, 1%THD+N at 2ohm PBTL and 200W, 1% THD+N at 4ohm BTL?
The TAS5634 can achieve 400W at 3ohm PBTL and 200W at 6ohm BTL which cannot meet customer's requirements.



Thank you and Best regards,

Wayne Chen
12/02/2020