Max recommended operating PVDD in the datasheet is 34V but the aaplication examples in section 8 show a 36V PVDD. What is the maximum PVDD for TAS5342A and what stops us increasign PVDD >34V for high impedance speakers for an increased output power?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Max recommended operating PVDD in the datasheet is 34V but the aaplication examples in section 8 show a 36V PVDD. What is the maximum PVDD for TAS5342A and what stops us increasign PVDD >34V for high impedance speakers for an increased output power?
Hi Jim,
Thanks for catching this disparity! I'll look into correcting the datasheet to fix this. I'd recommend sticking to the recommended PVDD voltages in the meantime.
What limits the PVDD max is the output FETs. If the voltage is too high then it risks damaging them.
Regards,
Robert Clifton
Hi Jim,
The biggest reason that abs max is quite a bit higher than the recommended max is due to current. The FETs can survive being at higher voltages but if you are trying to drive speakers at these levels you risk damaging the FETs from the current draw. At our recommended voltage levels, we have tested under normal use conditions that the current shouldn't damage the FETs but the same cannot be applied to the absolute max.
I hope that clarifies things.
Regards,
Robert Clifton