Hi team,
Would you please review the TPA3144 schematic and layout?
the output power request is 3W/8ohm. I will suggest customer to use the following setting.
1.PVCC=7.5V
2.Gain=36dB
3.LIMRATE=fast
4.LIMTHRES=1.193V
5.SSCTRL=SS OFF1
6.GVDD=6.91V. (it is from TPA3144 itself)
7. max input gain, limit to 320mV
Here is the schematic and layout file.
txn.box.com/.../5k4xpcxni0j98nluamacrxhhr0zrsfor
BR,
SHH