I want to use it at 2.5 Ohm, but can I use if I take care the peak current ?
In my plan, the peak current is 11 A. In the specification sheet, the shutdown detection current is 15 A.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you for your reply.
Power supply voltage : 25V
Max power output : 120W at THD10% , and 150W at THD30%
Hi Yagishita-san,
There are several limiting factors in your setup. The supply voltage being 25V will greatly limit the maximum power you'll be able to achieve. At 25V you would only be able to get about 105W out of a 3ohm load in BTL.
I would recommend using the TAS5614LA in PBTL mode if you want to get higher output powers using a 2.5ohm load and PVDD = 25V.
Best Regards,
Robert Clifton
Hello ! Mr Robert Clifton
Thank you for your strong support .
I would like to confirm that there is no problem even if I use it at 2.5 ohm.
Is there no problem even in the current state?