Other Parts Discussed in Thread: TAS3251, LMG1210, TAS5558, TAS5548
Hi,
Please recommend a PN to replace TAS5010 and TAS5342. These will be used in the new design of my customer. thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For your inquire:
There are two chips in their current design ,one is for I2S to PWM and another is a ClassD amp with PWM input. appreciate for the better solution.
power supply voltage? 24V or 40V
output power? 100W
Stereo mode or mono mode? Constant impedance amplifier is stereo mode. Constant voltage amplifier is mono mode(compatible with 70V and 100V)
Digital input or analog input? I2S ,Digital input
Speaker resistance? Not confirm yet. 8Ω first.
Hello,
I just need a recommendation about the replacement of TAS5010, my customer used this in "constant voltage power amplifier" before. but I can not find this part from TI website.
For "constant voltage power amplifier" EE, what is our recommended PN? thanks.
TAS5010's datasheet is as below. from it ,you can see it has I2S input and PWM out. in my customer case, they used PWM from TAS5010 to drive LMG1210.
pdf-file.ic37.com/.../TAS5010_datasheet.pdf