This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
While awaiting the promised additional info from Mr. Ravi Patil, I was asked by the system if the problem was solved. Unfortunately the "This did NOT resolve my issue" button did not work, so the case was closed.
Actually I still hope for further details from Mr. Ravi Patil. Thanks in advance.
Hi JH,
Based on your previous comments, you are able to see 24-bit I2S stream from the device when you analyze the output of PCM1861. However when you have TAS1020 as master and PCM1861 as slave, you are only seeing 16-bit. Is this the correct understanding of the issue?
It's highly unlikely that the USB-to-I2x interface is causing any issues here as we have not seen the same issue here or have heard it from other customers either. The likely issue could be w format selection for the windows driver. Please check the same and you should be able to see the 24bit data.
Hope this resolves the issue. If not, please let me know. Thanks.
Best regards,
Ravi