This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA2505EVM: PGA2505 App can't connect with EVM board

Part Number: PGA2505EVM
Other Parts Discussed in Thread: PGA2500EVM

Hi 

I using PGA2505EVM connect to PC with DB25 cable in EVM package,but there is no connection.

PC show LPT1 port in device manager,it loots no problem .

In the PGA2505EVM software , check "System information  " tab , message is " System information is unavailable at this time"

and retry with LPT2&LPT3 are the same .

PC OS is win 7

  • Hi Larson,

    I am getting a hold of the PGA2505EVM hardware by tomorrow. I will set up the device in the lab and get back to you ASAP. Please allow me a day to get back to you.

    Thank you,
    Luis
  • Hi Larson,

    Unfortunately, this evaluation board was released over 10 years ago and the legacy software is only compatible with Windows XP (or old windows versions) and the EVM interfaces through the parallel port (most standard USB to Parallel printer ports adaptors will not function).

    The PGA2500EVM/PGA2505EVM is in the queue schedule to be updated with new hardware/software; but these will not be released to production immediately.

    I will contact you directly via email with a possible workaround solution.

    Many Thanks and Regards,

    Luis Chioye