I have an issue with this IC. I placed a switch to shutdown the device manually, but the devices goes to DC FAULT each time I activate the shutdown switch AND the supply voltage is over 17V. If I lower to, lets say, 15V and cycle the shutdown switch, the error disappears and I'm free to increase the VCC to 24V and everything works fine, but in this case if I again use the shutdown, again the IC gos to DC fault. I'm not able to imagine what is going on.
Any help will be appreciated.
Julio Walter