This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6203A1: Problems with overheating and failing

Part Number: TPA6203A1

I am using the Device as per the data sheet. However we are getting the device over heating and failing. I do have a "heatsink via the base of the device soldered onto the pcb tracking, but not to anything else.It looks like thermal runaway. Can this happen?

If the soldering of the bottom of the ic is not soldered to Ground, can it fail? Is a 0.1uF on the Bi-pass pin 2 ok?

  • Hi Reg,

    Is the heating happening only during playback? Or is it happening also when there is no input signal?
    Have you inspected the output of the amplifier with a scope? Perhaps the device is oscillating at high frequencies and causing the excessive heating

    You can also share your design files so we can take a look. You can send an email to ivan.salazar@ti.com if you don't want to post it on the forum.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Hi Reg,

    Do you have further comments on the suggestions above?

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators