This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2505-Q1: Unable to get low quiescent current in shutdown mode

Part Number: TAS2505-Q1
Other Parts Discussed in Thread: TAS2505, TPS62740

Hi, 

We're using the TAS2505 Class-D amplifier in a low power portable device. The speaker will only be used during certain events and will be in low power mode for most of the time.

We were in the assumption that the quiescent current would be <5uA when the RST is pulled low, as shown in this table:

We're however measuring a increase of 85uA when we mount the TAS2505. The TAS2505 is connected to a STM32 microprocessor using I2C and I2S, as shown here:

As you can see we're using the internal LDO to generate AVDD and DVDD.

Can you help us with lowering the quiescent current from 85uA to the specified <5uA?

Thanks.