Other Parts Discussed in Thread: PGA2500,
Hi TIs,
Would you pls provide PGA2500 PCB file as gerb format? We also has a question on the R5&R6 in the evm sch ,such as how to adjust their value and what is their effort?
thanks a lot.
BR
Sara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TIs,
Would you pls provide PGA2500 PCB file as gerb format? We also has a question on the R5&R6 in the evm sch ,such as how to adjust their value and what is their effort?
thanks a lot.
BR
Sara
Hi Sara,
The PGA2500EVM provides a few non-populated resistor and capacitors as a configurable portion at its input for flexibility. Users are able to customize/prototype the input circuitry per the application requirement. The configurable portion of the input circuit includes R5, R6, R10, R11, R14, R15, CC1, CC2, and jumper JMP2. These components support prototyping of additional circuitry, such as pads and filters. During assembly at the factory, resistors R5 and R6 are not installed, while R10, R11, R14, R15, CC1, and CC2 are replaced by wire shunts.
I will need to check on the Gerber files, and if available, I will provide to you directly via email
Many Thanks,
Kind Regards,
Luis