This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5733LEVM: TAS5733L amplifier-supply Capacitor-type, ESR and outgassing

Part Number: TAS5733LEVM
Other Parts Discussed in Thread: TAS5733L

Hi,

I would like to know your thoughts on the choice of amplifier power-supply capacitor for the TAS5733L. Could you please advice?

I made a board that contains among other things the TAS5733L stereo reference design. Supply-voltage is 12V. The amplifier works flawless, I am really happy with it. I copied all BOM-parts and the schematic. The layout is my own, but resembles the reference-design on critical aspects.

However, I would like to encapsulate the pcba in epoxy, to make it like a brick. I am reading horror-stories about outgassing of electrolytic capacitors encapsulated by potting, which is the case for the Panasonic EEEFK1V221P capacitors that buffer the amplifier power supply in the reference design (C1,C2). Could you quantify the potential lifetime-impact in case of operating these 35V-rated capacitors on 12V, encapsulated in potting?

Now the obvious solution, as it seems to me, is to replace C1,C2 by polymer capacitors, such as Panasonic EEHZA1E221V : same capacitance (220uF), lower voltage-rating (25V), ESR way lower (27 mOhm instead of 160mOhm), same case-size 8x8. I do not see any drawbacks other than size and price, however I may be overlooking something. What are your thoughts?

Best regards, EJ