This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1802: BYPAS set on HIGH, but no DC component on DOUT

Part Number: PCM1802

Hi,

I making a project for school and am using the  PCM1802. I connected it and it works normal when I put something on the input (Analog output). Right now I want to see the difference when I set THE BYPAS on HIGH to see the DC on the output. Unfortunately It does not work ( it still only shows only the ANALOG). I even connected 2V to the input to have a pure DC input and it showed nothing on the DOUT. What can be the cause of that? Can it be solved?

Thank you in advance,

Filip