Other Parts Discussed in Thread: PCM1808, , TAS5421-Q1
The new problem is really to identify a way to connect a AQ100 (high temp) A/D converter to the TAS6421, with the minimal components as at temperature semiconductors become conductors. My initial idea of using the PCM1808 however, this is non ideal as requires an additional unwanted 5V supply. So, ideally i am looking for an A/D converter that will use the 3.3V supply from the TAS6421 and uses minimum number of components to generate timings for the TAS6421 to operate. Then i have to work out a way inorder to set up I2C without microprocessor as this will needed to be thermally tested before software team get allocated to the project. The TAS6421 is begging to be a night mare device any idea how one might overcome some of these obtickles? Thanks in advance.
victor