This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1662-Q1: issue about output pin blocked -VEE

Part Number: OPA1662-Q1
Other Parts Discussed in Thread: NE5532, , OPA1664, OPA1662

We have replaced a ne5532 with OPA1662-Q1. The circuit is a simple voltage follower with a capacitive load to decoupling output.

We didn't have problems with the ne5532.

With the opa1662-Q1 we have some broken devices: output pin blocked to -VEE. None particular stress to cause the broken.
Do anyone have already knoledge about this critical aspect of this AO? Any suggest?

  • Hello Stefano,

    Thank you for your post. I can help you.

    Can you share with me the following so I can help analyze your circuit:

    • What are the supply rails?
    • What is the input signal? 
    • What is the expected output signal?

    The issue is that the output is railing to -VEE, is that correct?

    -Tamara

  • Hi Tamara,

    The supply rails are +15V -15V nominal.


    The input signal come from an OPA1664, same supply rails (+-15V), signal max level 14dBu, 20-20KHz (audio signal). No (or very low) DC.


    The output signal expected is the same from input: it isn't expected any amplification. The stage could fit a resistor for a 6dB amplification, not fitted.


    Yes, the output is railing to -14V (locked to -14V)
    I attach an input signal, output signal of the broken AO (pin1), signal on pin 3 (note the DC component of -4.4V, from -15V). (On pin2 the signal is the same of pin3 but a DC component of -5.1V)

    Thank you for your support.

    Best Regards

    Stefano

  • Hi Tamara,

    any updates on this issue? It still remains.

    Regards

    Meroni Stefano

  • Hello Meroni,

    I built this circuit in TINA Spice so I can analyze the nodes more carefully. The circuit seems to be behaving as expected. You can see my circuit and the transient analysis.

    Can you try swapping out the OPA1662 you have with another one and sharing the results?

    OPA1662 TINA.TSC

    -Tamara

  • Hello Tamara,
    thank you for your reply.
    Here are the waveforms get with a not broken OPA1662.

    They look like the waves obtained by your simulation.

    Regards

    Stefano Meroni

  • Hello Stefano,

    Looks like the OPA1662 you were originally using was damaged. With a good OPA1662, the circuit behaves as expected. I will close this thread now.

    -Tamara