Other Parts Discussed in Thread: TAS2555, TAS2563, TAS2557, PCM4201
Dear support Team,
What must i do to setup the TAS2555 for analog input?
Apparently i cannot select this input option in the PPC3 software, so i have made some research about
how to set up the TAS2555 by hand. But i am not successful, the speaker is still silent.
- Analog input is done via the Vsense ADC.
- I have manually set P0B0R8 to 0x01 to enable analog input via the Vsense ADC
- I have checked power control register P0B0R5 to be set to 0xa3. Seems ok, D0 showse V-sense ADC powered.
- I have checked power flag register P0B0R100 to show 0xf0.
That's contradicting the settings in P0B0R5...
How to proceed to use analog inputs?
Kind regards
Andreas Paulin