Other Parts Discussed in Thread: TPA3126D2
Hi Audio team,
I have questions about class-D for following requirement.
Mono/Stereo: Mono
Input: Analog in
Output: BTL
PVDD: 8V
Power: 16~20W with 10% THD+N
Could you help below questions?
[Question 1]
Do you have any data that shows TPA3112D1 can output 16~20W with 10% THD+N from 8V, or how much TPA3112D1 can output with 10% THD+N from 8V?
[Question 2]
In addition, do you have any other recommended devices for above requirement?
[Question 3]
When I take a look at some datasheet like TPA3126D2/3128D2, these support PBTL.
However, these datasheet describe 10% THD+N maximum output power from 8V is 12W at 3RL.
TPA3126D2 figure 24.
From below calculation, possible output power seems to be 170W but why TPA3126D2/28D2 max output power is limited by 12W?
8V PBTL configuration is 32Vpbtl(22.6Vrms)
P=V^2/RL=170W
Regards,
Kai