Hi Team,
I made my customized bourd with TAS5721, with I2S input, and drive a headphone and two speakers.
The I2C communication is good, and the board works perfectly with two 5W speakers, but has no output on headphone.
my registor setting as below:
X1B 00 ! Factory trim
X21 00 00 42 03 ! Set SubChannel Mixer to (L+R)/2
X05 84 !Exit Shutdown and configure the device in 2.1 Mode
X07 30 !Set MAster Volume to 0dB
Would you please advise how to switch the output to headphone? sorry I didn't find it on the datasheet.
Thanks.