This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1753: Pop noise issue during power-up

Part Number: PCM1753

Hi,

Could you please tell me the root cause and workaround regarding the pop noise issue during power-up?
I found the link of the FAQ in the following post, but the link has already been lost.

PCM1754DBQR questions about POP noise and mute function
https://e2e.ti.com/support/audio/f/6/t/487134

Best regards,
Kato

  • Kato-san,

    I apologize for the delay but we will get back to this and your other two threads by tomorrow US time.

  • Hi Kevin-san,

    Thank you for your reply.

    For PCM1753 questions, I am looking forward to getting the detailed information from you tomorrow.

    Best regards,
    Kato

  • Hi Kato-san,

    You have a few threads open about this topic, so the answers will probably be similar in each one. 

    The PCM175x is an older device and it does not have much clock error protection circuitry.  There is a risk of a pop noise whenever the delta-sigma modulator starts or stops, or when there is a clock error.  Basically, when the DSM is switching, there is no sudden DC change (besides those desired from the digital input source), but if there is a clock error, the DSM stops.  During a stop, the ~7 current segments go to a DC state, that can be different than the VCOM voltage.  This abrupt stop can sound like a pop or glitch if the magnitude is large enough.  

    The only way to avoid this is to implement an external mute functionality that can be asserted when there is a clock error, but that error detection would need to come from the I2S source rather than the PCM175x.

    Thanks,

    Paul

  • Hi Paul-san,

    Thank you for your support.

    I understand.

    Best regards,
    Kato