I am designing a 5.1 channel audio system using 3 TPA3125D2 amplifiers. The subwoofer has it's own amplifier and will be driven directly from the preamp on my board, meaning that one of the channels will be driven with no load attached. There is also the possibility of other speaker combinations where one or both amplifiers on a given chip may have no load. Putting the unused amps into shutdown is not feasible as that would shut down both channels including the one being used. I have found conflicting information as to whether it is safe to run a class D amplifier with no load, with some saying that the output LC filter can create voltages high enough to damage the amplifier. Is it safe to run with no load attached, and if not then what can be done to make it safe? Is it as simple as placing schottky diodes from each output to the power rails to prevent the voltage generated by the filter from exceeding the power supply by more than one diode drop?