I've implemented a stereo 50W amplifier design using the TPA3126D2 amplifier chip. I'm having an issue passing CISPR25 radiated emissions. Initially I was operating the chip at 400KHz, but while the fundamental falls in a gap band of CISPR25, the second harmonic exceeds the class 2 limits by about 12dBuV/m. I switched to the 1.2MHz operation, but now have an issue with the 5 harmonic failing in the 6MHz band. Here's the schematic of amplifier section: