Other Parts Discussed in Thread: PCM6240-Q1
Hi Sir,
I attached our audio DSP/AMP/ADC converter block diagram.
The power in of the class D AMP is 20V, so the VDD of speaker out is 10V that is over the analog input power of PCM1808.
Does the VinL/R spec of the converter exceed 10V? Is there a recommended model?
Or recommend a RC circuit can be add in front of the analog input that does not exceed VinL/R spec.
B.R.
Ken