Other Parts Discussed in Thread: LM317,
Okay, I had the same issue with the RESET line and verified that applying an external 5V on RESET started the part. This is mentioned in the forum here. (Nick and Luis contributing.)
However, I do not have a 5V supply in the design I was doing. Can I use a simple resistor divider with my 30 volt supply to generate 5 volts for the RESET pullup? Or do I need a more elaborate scheme. i.e. add some sort or regulator powered off the 30 volts?
Thanks in advance.