The analogue part of my project is bipolar, so Vdd is +5V, Vss is -5V, and analogue ground is 0V.
Can digital ground be Vss? or must it be 0V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The analogue part of my project is bipolar, so Vdd is +5V, Vss is -5V, and analogue ground is 0V.
Can digital ground be Vss? or must it be 0V?
Hi, Ian,
Yes, the digital ground can be VSS. However, I would recommend to join both digital and analog planes with 0-ohm resistors or single PCB traces. This is a good practice to reduce digital noise on the analog portion.
I hope this helps you. Please let me know if you have additional questions or comments.
Best regards,
Luis Fernando Rodríguez S.
If the digital ground is Vss and the analogue ground is 0V, then joining them with zero ohm links isn't going to be a bit hard on the power supply!
Hi, Ian,
Sorry for the confusion, I made a mistake on my previous post. Yes, the logic level would be 0V. Then, this digital ground plane can be connected to the analogue ground plane through a 0 ohms resistor or single PCB traces.
Best regards,
Luis Fernando Rodríguez S.
Luis Fernando Rodriguez S. said:Then, this digital ground plane can be connected to the analogue ground plane through a 0 ohms resistor or single PCB traces.
Why is this outmoded and frankly bad advice -- two ground planes connected with a jumper or small trace -- still being given?
Pour one ground plane. Then "partition" the routing -- that is, route digital traces away from analog. Always mind where the return current flows.
See, for example, Henry Ott's papers and books about this.
Logic is between 0V and VSs.
Because the logic output has to drive a 12V indicator panel, and the LM1972 can't manage +/-12V supplies, so I'm using +/-6V for the audio.
The logic can operate at any level, so if I put it between 0V and -6V it can directly drive a ULN2003 which switches the indicator panel.
If the indicator panel is on 0V/12V then I need an extra supply. If the logic is between 0V and +6V then I have to logic-shift the output to the ULN2003.
That's why.