This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6166A2: Question of TPA6166 Schematic Designs on Jack_Sense and Mic Output

Part Number: TPA6166A2
Other Parts Discussed in Thread: TS3A227E

Hi Sirs,

As title, we have two questions of schematic design of the TPA6166 which need product line's suggestion:

1. Can we leave MOUNT open and connect C3 to GND for Single-Ended mic design?

 

2. Do we need an inverter on JP1 when using a phone jack with normal open detection design (similar to Q1 on the TS3A227E EVM)?    
3. Is there internal pull up or pull down with the JACK_SENSE pin? Can we connect the JACK_SENSE to SOC's GPIO?






Thank you and Best regards,

Wayne Chen
07/17/2020