This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi
I want to know TLV320DAC3101's power consumption with specific voltage condition when it plays sound.
condition : playback to 8Ohm stereo speakers, slave mode(0dB FS 1kHz signal)
example :
AVDD 3.3V, ?? mA, SLVDD 3.9V ?? mA, SRVDD 3.9V ?? mA, HVDD 3.3V ?? mA, DVDD 1.8V ?? mA, IOVDD 3.3V mA
total power consumption is ?? mW
Hi, Jeonghwa,
Please take a look at this Application Report. It contains the information that you are looking for.
https://www.ti.com/lit/an/slaa468b/slaa468b.pdf
Best regards,
Luis Fernando Rodríguez S.
Hi Luis
Thanks for your reply.
I already checked the application note before you let me know.
But I thought the document hadn't the information of power consumption with playing sounds.
According to 2.1 Test Setup on the document, after the sound is stopped, the current measurement is taken.
Could you check it?
I want to know the power consumption with specific voltage condition when it plays sound.
condition : playback to 8Ohm stereo speakers, slave mode(0dB FS 1kHz signal)
Hi, Jeonghwa,
Thank you for providing the additional test conditions.
Please find the current measurements for each power supply below:
AVDD:2.95 mA
SLVDD: 11.5mA
SRVDD:24.3 mA
HVDD: 7.11 mA
DVDD: 2.93 mA
IOVDD: 10uA
Best regards,
Luis Fernando Rodríguez S.
Hi Luis
Thank you for your support.
According to your result, TLV320DAC3101 consume only total 178.125mW when it play sounds with playback to 8Ohm stereo speakers, slave mode(0dB FS 1kHz signal).
Am I correnct in understanding ?
I want to check one more clearly due to very small power consumption.
item / voltage V / current mA / mW
AVDD / 3.3 / 2.95 / 9.735
SLVDD / 3.9 / 11.5 / 44.85
SRVDD / 3.9 / 24.3 / 94.77
HVDD / 3.3 / 7.11 / 23.463
DVDD / 1.8 / 2.93 / 5.274
IOVDD / 3.3 / 0.01 / 0.033
SUM / 178.125
Hi, Jeonghwa,
I apologize for my late response. We have faced many issues on E2E and we lost some threads. I retook the data in order to verify the current for SPLVDD and SPRVDD. You were correct, these values were for a no load connection. The current values that I got with the 8ohms loads are:
AVDD = 12.1 mA
SLVDD = 47.3 mA
SRVDD = 48.2 mA
HVDD = 17.7 mA
DVDD = 2.93 mA
IOVDD = 10 uA
These values result in a power consumption of 476 mW. The output power results in ~420 mW under these conditions.
Please let me know if you have additional questions or comments.
Best regards,
Luis Fernando Rodríguez S.