This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Usually we havent silent periods, but if we use the mute option, we have between 1-3 seconds on muting after we unmute the device. If we dont active the mute, we could all the time play music, but for save energy and reduce the dissipation, because the device is 99.99% time off, we would mute this. Could we know, the the device is ready?
We have connect the TPA in 36db config, Mono function and differential feed from other preamplif (8002A with other power (3.3V) with two 1uF condensators in serie to uncouple the dc voltage (in case of...).
Would be a cause of time of charging decoupling caps?
Hi,
I am sorry. I can not fully understand what your mean.
Do you mean that you want to mute device most time, and know if device is ready?
And second question, could you please give me more detail information?
Regards,
Derek