Hi,
Currently I don't have TAS2110EVM and I need to get a simple setup file for playing audio using I2S bus. Can I use PPC3 to generate a setup file without an EVM? For example if I set some options in "Device Control" does it transfer to "End System Integration" (see the image below) of the PPC3 to dump all register data?
At this stage I just need to play audio using I2S bus.