This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101EVM-K: Firmware upgradation failed

Part Number: TLV320ADC3101EVM-K


Hello ,

I tried the steps in the word file and still I was unable to fix the problem. Getting error Download command failed.

When I m connecting the EVM USB,

W11 disconnected

J6 1 and 3 connected

SW2 = A2  and external MCK OFF rest all ON

D2 is not glowing

Device manager  - shown as unknown device

If i connect the device with all the appropriate settings, SW2 A2 as OFF and W11 as connected . I m getting BSOD usbaudio.sys kernel trap mode !!

0513.USBEVM_Revive.docx