I have an issue with about 10% of the DRV134 Audio-Balanced Line Drivers. On about 5 to 10% of the units tested the THD + N level is an order of 10 times higher than the published specification. Most of the parts perform as published with a nice flat noise floor when swept from 20 to 20KHz.
We are testing the parts with a Audio Precision System one audio analyzer. The test frequency is 1,000 Hz with the bandwidth set from 22 to 22,000 Hz at 0 dBm level. For good parts we are measuring a THD + N on the average of 0.001 % while bad parts are typically 0.01 % tested at 1,000 Hz.
Confidentially, we had the same issue back in 2004 when the part was available from Analog Devices as the SSM2142 At that time Analog Devices stated " We did have a serious manufacturing problem with the part last year which should be resolved by now ". Analog Devices had then resolved the problem and all the parts after that date until now worked as expected. Since they resolved the issue in 2004 we have continuously used 10,000 + of this part with no issues. I do not know if your DRV134 is the SSM2142 rebranded but it sure seems to have the same issue.
Please get back to me on that as soon as possible as we have a production run shut down awaiting a response.