This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Total Icc current consumption specification is 18mA(typ) @44.1KHz on the datasheet.
There are 3pins(#15,#23,#28) connection for analog Vcc +5V power supply.
Our customer try to add independent noise de-cupping RC filter for each pin to achieve the best quality sound.
Their question is what is current consumption of #15 Vcc2R and #28 Vcc2L at fs=44.1KHz?
Regards,
Mochizuki
Hi Mochizuki-san,
Unfortunately, I do not have that data. I expect that the majority of the 18mA will flow equally to the VCC2R and VCC2L pins, as they controller, the delta-sigma modulator switching and current sources. The VCC1 pin is the DSM reference current, so will be lower.
Thanks,
Paul