This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5558: i get only 192kHz PWM Output

Part Number: TAS5558
Other Parts Discussed in Thread: TAS5548

Hi, im currently designing an 7.1 AMP with PSVC inkl. Subwoofer an i have problems with the TAS5558.

I2C Connection works as expected and i get ACK´s. The 3V3 power is stable. On pin 11 MCLK i have an 12,288MHz Oscillator and 10k on pin 12 (18k dont work)

My INIT I2C sequence is:

1. 0x12 = 0x00

2. 0x03 = 0xA0

3. 0xE0 = 0x00 0x00 0x00 0x04

4. 0xD9 = 0x00 0x00 0x00 0x48

5. set /MUTE pin HIGH

after that i VALID HIGH and PWM out, Audio is working fine but only 192kHz PWM?

Is there someting miss configured ?

greatings from germany