This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
PCM1789 replace AKM4388,We found that the phase of the high-pitched and low-pitched AUX channel of the PCM1789 prototype is basically the same, while the phase of the high-pitched and low-pitched BT channel is quite different.The figure is shown below.What parameters need to be set to affect the delay and phase in PCM1789?
Hi Smith,
The register settings should not affect this. Do you have any output filtering? The phase response almost looks like the there is a low pass filter at ~3kHz. Is the amplitude vs frequency response the same?
Thanks,
Paul
Hi Smith,
Is the amplitude vs frequency response the same?
I see there is a simple low-pass filter on the output (1kΩ, 820pF||820pF), but is there any additional load on the output?
Thanks,
Paul