This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6166A2: Is the TPA6166's IRQ# An Open Drain or Push-Pull Signal?

Part Number: TPA6166A2

Hi Sirs,

As title, is the TPA6166's IRQ# an open drain or push-pull signal? We assume that it is an open drain signal because the datasheet does not specify VOH(min) and there is a 100kR pull up to 1.8V on its EVM. However, there is no pull up resistor on the reference design on the datasheet. Would you pls confirm if that if the pull up resistor on IRQ# mandatory? Is there internal pull up with the IRQ#

TPA6166 EVM Schematic  


TPA6166 Datasheet







Thank you and Best regards,

Wayne Chen
12/08/2020