I am using the TAS5713 in a PBTL configuration and had requested TI tech support insofar as the proper electrical connections. I received the attached drawing showing the connections. I have the TAS5713EVM board which is wired as 2 BTL (stereo) outputs and have noticed that the PCB layout for the boost capacitors on each output were very deliberately connected right at the output filter. Should I followd a similar approach in the PBTL layout, i.e. keeping the OUTA/OUTB and OUTC/OUTD wiring connections separate up to the output filter, as well as the boost capacitor connections for each of these 4 outputs? Does anyone have a sample board routing (i.e. tested) for the TAS5713? connected in PBTL mode ? I'd like to only have to do this once!
Thx,
Dave