The FAULT pin is all the time on low and therefore i get no output on the Speaker. I only connected one speaker to one output terminal, the rest of the outputs stay unconnected. Also only one input is connected.
I already read it could be a problem with the Inductor, but the used inductor has more or less the same specification as the one used in the Evaluation Module. It is a Bourns SRN8040TA-220M with 220 uH and and Current Rating of 2,9A.
The RESET pin deliveres a high signal.
There is a screenshot of the schematic: