This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What uF can be connected to VCOM-AGND of PCM1804? I want to attach a value larger than 0.1uF. For example, 10uF or 100uF
Hi Masahiko,
We recommend a value of 0.1uF only and do not have data for higher values capacitors. I would be careful using excessively large capacitors though as this could potentially make the VCOM voltage unstable. These pins typically only have a few hundred microamps of drive strengths so excessive capacitance can also delay startup time.
Best,
Zak