This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1754: Can PCM1754 operate with non-audio related sampling frequency?

Part Number: PCM1754

Hello Team, 

I would like to operate PCM1754 with non-common-audio related sampling frequency. (Except for 44.1kHz, 48kHz, 192kHz and so on.)

For example, In case of fs=70kHz, BCK= 64*fs=4.48MHz, and SCK=128*fs=8.96MHz, Can PCM1754 work correctly?

thanks.