Other Parts Discussed in Thread: TLV320AIC3104
Hi
I need information for Minimal register configuration for TLV320AIC3104 playback.
AIC3104 is configured in master mode.
Is it possible to use AIC3104 without MCLK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLV320AIC3104
Hi
I need information for Minimal register configuration for TLV320AIC3104 playback.
AIC3104 is configured in master mode.
Is it possible to use AIC3104 without MCLK?
Hi, Saurabh,
Please take a look at the following script.
# BCLK = 1.536MHz; WCLK = 48kHz # MCLK = 24.576MHz # # Page 0 w 30 00 00 # # Software reset w 30 01 80 # # PLL Programming (Q = 4) w 30 03 20 # # Clock Register w 30 65 01 # # Master mode w 30 08 c0 # # Codec Data-Path Setup w 30 07 8A # # DAC Power and Output Power Control w 30 25 C0 # # DAC Output Switching Control w 30 29 02 # # Left-DAC Digital Volume Control w 30 2B 00 # # DAC_L1 to LEFT_LOP/M w 30 52 80 # # DAC_R1 to RIGHT_LOP/M w 30 5C 80 # # LEFT_LOP/M Output Level w 30 56 09 # # RIGHT_LOP/M Output Level w 30 5D 09
The TLV320AIC3104 BCLK and WCLK will be configured as outputs in master mode. So, it is necessary the usage of the MCLK.
Best regards,
Luis Fernando Rodríguez S.
Hello, Saurabh,
The distortion problems are often related with the clocking configuration. However, the register configuration related with the sampling rate is correct.
Also, this kind of problems is related with power supply sequencing and ground planes. The analog activity must be separated from the digital activity. So, we suggest to separate the analog ground plane from the digital ground plane and join them in one point. Also, could you provide information about the power supply sequencing? See 12 Power Supply Recommendations section for details.
Best regards,
Luis Fernando Rodríguez S.